Energy Efficiency


                   
                   
                   

                  Solutions by segment

                   
                   

                  To limit energy cost and its impact on environment we must learn to adapt and manage energy consumption, cost  and pollutant.

                  Industry & Infrastructure: a key target especially around motors

                   
                   

                                 Over 30% of the consumed energy. Motors account for 60% of the electricity usage. Average facility can reduce energy consumption by 10 to 20%.
                   

                  > Electrical Energy 
                  > Water                                              

                  > Oil & Gas 
                  > Mining, Minerals & Metals 



                   
                   

                  Data Centres & networks : the most sensitive market

                   
                   

                           About 48% projections data centres costs are dedicated to energy.
                  Simple changes to the way approaching energy use can help recoup losses !
                  > Data Centres 


                   
                   

                  Buildings : the biggest consumer

                   
                   


                                Over 40% of the consumed energy. 
                  3 key areas : HVAC, lighting & integrated building solutions. Renovation can yield up to 30% of energy savings.
                  > Hospitals 
                  > Hotels  
                  > Offices
                  > Retails 


                   
                   

                  Residential: high potential of saving!

                   
                   

                      20% of the consumed energy.
                  10 to 40% electricity saving using energy efficient products.


                   
                   
                    
                   
                  To know more

                  To know more 

                  Requests for Solutions, Products and Services information

                  Telephone : 1-800-565-6699

                   

                  Key downloads