Mining, Minerals, Metals


             
             
             

            Application: Pumps & Fans Control (Industry/Infrastructure)

             
             

            Pains & drivers

            • In Industry, 70% of electrical consumption is used to turn motors. Of these motors, 33% of them control pump or fan applications.
            • Most pump and fan applications are driven by a DOL solution of SoftStarter. This means that the motor runs at full speed and the flow variation is obtained. The energy consumption falls very little when the flow decreases. At 80% of the nominal flow, the energy consumption remains at 95%. The potential for saving on the installed base is huge.
            • The CEMEP association has made a simulation for the European market. The use of Drive in such applications could save 900 M Euro/year as well as 4 Million tons of CO2/year.

            How can a customer manage energy more efficiently?

            • To save energy you must:
              - drive the motor with a frequency inverter instead of a contactor or Soft Start
              - remove the restriction device (valve or damper)
            • The AC Inverter allows you to adjust the speed of the Pump or the Fan, and therefore the Flow
            • The result is huge savings compared to conventional solutions:
              - up to 50% for Fan , return on investment for the drive is within one year
              - up to 30 % for a Pump , return on investment within 2 years

            Solutions or architectures used in the application

             

             
            A) Solution without Drive
            The motor turns at a fixed speed according to the network frequency and the number of poles.
            Example : 3600 Rpm for 60 Hz
            Motor 2 poles
            The only way to adjust the Flow is a restriction device (damper) which generates losses.







            B) Energy Saving Solution with Drive
            The Drive, which is also called a frequency inverter, lets you vary the frequency and therefore the motor speed, too.
            The Flow is directly proportional to the speed.
            The damper or valve are no longer required.







            C) Energy Consumption with and without Drive
            Example for Fan Application

            Outlet damper
            Variable speed drive
            50% of energy saving at 80% of the nominal flow


            Example for Pump Application

            Control valve
            Drive
            30% of energy saving at 80% of the nominal flow 

              
             
            To know more

            To know more 

            Requests for Solutions, Products and Services information

            Telephone : 1-800-565-6699