Offices


               
               
               

              Application: Lighting Control

               
               

              How can a customer manage energy more efficiently?

              • Lighting can represent up to 40% of energy consumption in buildings depending on segments.
              • Lighting control is definitely one of the easiest ways to save energy costs on one of the most common applications. Applying an effective lighting control solution, users can easily save up to 50% on their electricity bill compared to traditional ways.

              Solutions or architectures used in the application

              • The solution provides automatic means to optimise lighting based on the 3 main parameters indicated above (time, intensity and presence), alone or combined.
              • The solution can begin from very local and small solutions, such as timers, up to very sophisticated, customised but flexible, centralised solutions as part of building automation systems.
                
               
              To know more

              To know more 

              Requests for Solutions, Products and Services information

              Telephone : 1-800-565-6699