Oil & Gas


                     
                     
                     

                    Application: Pumps & Fans Control (Industry/Infrastructure)

                     
                     

                    Pains & drivers

                    • In Industry, 70% of electrical consumption is used to turn motors. Of these motors, 33% of them control pump or fan applications.
                    • Most pump and fan applications are driven by a DOL solution of SoftStarter. This means that the motor runs at full speed and the flow variation is obtained. The energy consumption falls very little when the flow decreases. At 80% of the nominal flow, the energy consumption remains at 95%. The potential for saving on the installed base is huge.
                    • The CEMEP association has made a simulation for the European market. The use of Drive in such applications could save 900 M Euro/year as well as 4 Million tons of CO2/year.

                    How can a customer manage energy more efficiently?

                    • To save energy you must:
                      - drive the motor with a frequency inverter instead of a contactor or Soft Start
                      - remove the restriction device (valve or damper)
                    • The AC Inverter allows you to adjust the speed of the Pump or the Fan, and therefore the Flow
                    • The result is huge savings compared to conventional solutions:
                      - up to 50% for Fan , return on investment for the drive is within one year
                      - up to 30 % for a Pump , return on investment within 2 years

                    Solutions or architectures used in the application

                     

                     
                    A) Solution without Drive
                    The motor turns at a fixed speed according to the network frequency and the number of poles.
                    Example : 3600 Rpm for 60 Hz
                    Motor 2 poles
                    The only way to adjust the Flow is a restriction device (damper) which generates losses.







                    B) Energy Saving Solution with Drive
                    The Drive, which is also called a frequency inverter, lets you vary the frequency and therefore the motor speed, too.
                    The Flow is directly proportional to the speed.
                    The damper or valve are no longer required.







                    C) Energy Consumption with and without Drive
                    Example for Fan Application

                    Outlet damper
                    Variable speed drive
                    50% of energy saving at 80% of the nominal flow


                    Example for Pump Application

                    Control valve
                    Drive
                    30% of energy saving at 80% of the nominal flow 

                      
                     
                    To know more

                    To know more 

                    Requests for Solutions, Products and Services information

                    Telephone : 1-800-565-6699

                     

                    Success Stories