Technical FAQs

Ask a Question

What is the maximum number of simultaneous sockets supported by the embedded Ethernet Twido controllers?

The embedded Ethernet Twido controllers support 4 simultaneous TCP/IP sockets. It also allows one marked IP connection, as configured

in the TwidoSoft application program.
Was this helpful?
What can we do to improve the information ?