Technical FAQs

Ask a Question

Which Quantum power supplies can be used in a Quantum SIL2 Safety System?

Issue
Power supply certified for safety application

Product Line
Modicon Quantum

Resolution
Only the Quantum 140CPS12420 power supply is certified for use in safety applications.

Was this helpful?
What can we do to improve the information ?