Technical FAQs

Ask a Question

How do I print my project using TwidoSoft v3.5?

Goals and Symptoms

This resolution is to show how to print a project using TwidoSoft V3.5.

Causes and Fixes

First, launch TwidoSoft and open the project you would like to print. Now open "Print configuration"
which is under the File menu (see below for illustration).



Once the Print configuration window is open, you need to choose which options you want to print then
click the Print button ( see below for illustration).


Once the print button is pressed, the print popup window will appear. Confirm which printer you are looking to print from
and click on the OK button (see below for illustration).


Was this helpful?
What can we do to improve the information ?