Technical FAQs

Ask a Question

Does the 140XBE10000 Quantum backplane extender module come as a kit or are the components sold separately?

Issue
140XBE10000 sold as a kit or separately 

Product Line
Modicon Quantum

Resolution
The 140XBE10000 Quantum backplane extender module are sold separately and you also need to purchase the extender cable (see below).
140XCA71703 Quantum backplane extender cable, 3 ft, 1 m
140XCA71706 Quantum backplane extender cable, 6 ft, 2 m
140XCA71709 Quantum backplane extender cable, 9 ft, 3.1 m

Was this helpful?
What can we do to improve the information ?