Technical FAQs

Ask a Question

How do I correct the Control Expert (formerly Unity Pro) error which generates the message "The system cannot animate so many screens. Please close some of them."?

This error can be corrected by selecting the  PLC Set Address Bandwidth window.
The default parameters are
"Animation support" = 70
"PLC Monitoring" = 10
"PLC Screen "= 10
"Diagnostic "= 10.


Please see the "Procedure for accessing bandwidths" section of the attached Control Expert (formerly Unity Pro ) Help document.
Bandwidth_comm_parameters.zipBandwidth_comm_parameters.zip


Legacy KB System (APS) Data: RESL212697 V1.0, Originally authored by DaSo on 10/08/2013, Last Edited by DaSo on 10/08/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?