Technical FAQs

Ask a Question

How to show the number of times variables are used in a Unity pro application.

Issue:
To inform the user how to show the number of times variable are used in a Unity Pro application.


Product Line:
Unity Pro software


Resolution:
Step 1. Right click on the area where the arrow is pointing


Step 2 Select the " Customize Column "

Step 3. select the " Used" option, then select OK


This option will show the number of times variables are used in the program and in other parts of the project (animation tables, user windows).

Was this helpful?
What can we do to improve the information ?