Technical FAQs

Ask a Question

Why do I get the error message "There are not enough I/O words configured to add this module. Please increase the amount of I/O words in the configuration if possible." when trying to save my Traffic Cop configuration in the ProWORX 32 programming software?

Issue
"There are not enough I/O words configured to add this module. Please increase the amount of I/O words in the configuration if possible."

Product Line
ProWORX 32

Resolution
This error will occur because you don't have enough I/O words configured in the project configuration. Open the ProWORX 32 Configuration Controller Properties.


Increase the I/O Words and save the new Configuration. You can now go back into the Traffic Cop, add the modules and do a save without getting the error message.

Was this helpful?
What can we do to improve the information ?