Technical FAQs

Ask a Question

Why does the HMIG3U have intermittent download failures?

Issue:
Why does the HMIG3U have intermittent download failures?

Product Line:
Vijeo Designer (SP4 or older), HMIG3U all revisions

Resolution:
The HMIG3U's general cpu load is heavier than that of XBTGT or HMIGTO. For this reason, there sometimes maybe intermittent download failures over Ethernet or USB cable. A fix for this issue will be released in Vijeo Designer V6.2 SP4.1 and later.

This verison will improve performance of the HMIG3U so that CPU load is properly distributed across two cores. System processes such as download will be given highest priority.



 
Was this helpful?
What can we do to improve the information ?