Technical FAQs

Ask a Question

Why will the 8839 E-Flex not start in auto mode?

Issue:
Why will the 8839 E-Flex not start in auto mode?

Product Line:
8839 EFD 

Environment:
All

Cause:
​The drive runs in hand and bypass not in auto mode? 

Resolution: 
Verify the auto start contact is closed between Pin 7 and Pin 6.
Verify 120Vac  at the RCR relay pin 6.
Verify the drive is not in a fault state.
Was this helpful?
What can we do to improve the information ?