Technical FAQs

Ask a Question

What are the specifications on the ATV320 Internal +24Vdc power supply?

Issue: 
What are the specifications on the ATV320 Internal +24Vdc power supply?

Product Line:
Altivar 320

Environment::
All serial numbers 
 
Cause:
Installation / Setup

Resolution:
+24 Vdc Output power supply for
digital inputs

Tolerance: –15...+20%
Current: maximum 1.1 A
Was this helpful?
What can we do to improve the information ?