Technical FAQs

Ask a Question

What is the 200 mm shaft used for VLS3P032R1 switch and VLSH1S5B handle?

Issue:
What is the 200 mm shaft used for VLS3P032R1 switch and VLSH1S5B handle?

Product Line: 
Operating Mechanism and Disconnect Switches

Environment:
North American Products

Cause:
​Would like to order the switch in pieces

Resolution:
Only available in VLSS1505 (150 mm) 
and VLSS3005 (300 mm). 

VLSS2005 (200 mm) is not recognized on Q2Cash Tool.

It was decided not to market the 200 mm shaft as the 300 mm can be cut down if needed. 
Reference: 9400CT1601

 

Was this helpful?
What can we do to improve the information ?