Technical FAQs

Ask a Question

Are Powerpact H, J, and L Frame breakers available with ERMS?

Issue:
Is ERMS an option with Powerpact H, J and L breakers?

Product Line:
Circuit Breakers

Environment:
Powerpact H, J, L Circuit Breakers

Resolution:
ERMS is not offered with the Powerpact H, J or L frame circuit breakers. 
ERMS is available for the Powerpact P, R, and Masterpact NT and NW breakers, with P or H trip units.
Was this helpful?
What can we do to improve the information ?