Technical FAQs

Ask a Question

Can the Conduit kit be purchased separately for the ATV600 / ATV900 series drives?

Issue:
Can the Conduit kit be purchased separately for the ATV600 / ATV900 series drives?

Product Line:
ATV600 and ATV900 series drives.

Environment:
All models and serial numbers, frame size 4 and below.

Cause:
Information not available in current literature.

Resolution:
For frame size 4 and below, the Conduit kit is attached to the drive when purchased.  It is not available for purchase as an individual component.  For frame size 5, the conduit kit is included with the drive purchase but ships separately.  For frame size 6 and above, the conduit kit is not included and must be purchased separately, if needed.
 
Was this helpful?
What can we do to improve the information ?