Technical FAQs

Ask a Question

Difference between XY2CE***** and XY2CE*****H7

Issue:
What is the difference between XY2CE1A250 and  XY2CE1A250H7
 
Product Line:
Machine Safety Products
 
Environment:
North American Products
 
Cause:
Would like to know if they can have the XY2CE1A250H7 instead of XY2CE1A250 as the latter is not in their stock.
 
Resolution:
They are electrically and functionally the  same. The  only difference is the cable entry.  Without the H7 - 3 plain hole for Pg 13.5 or ISO M20 cable gland.
With the H7 - 3 tapped entry 1/2" NPT conduit entry.
 
Was this helpful?
What can we do to improve the information ?