Technical FAQs

Ask a Question

How do you change the IP address on the ATV58 drive with an Ethernet option card?

Issue:
How do you change the IP address on the ATV58 drive with an Ethernet option card?

Product Line:
ATV58

Environment:
All 

Cause:
Needs to set up the IP address on the ATV58 drive. 

Resolution:
P05= 11 to enter the IP address.

P01= IP1
P02= IP2
P03= IP3
P04= IP4
Was this helpful?
What can we do to improve the information ?