Technical FAQs

Ask a Question

XB4BD912R and XB5AD912R Wiring

Issue:
Is there a diagram for wiring the 22mm potentiometers, XB4BD912RxxK and XB5AD912RxxK units?

Product Line:
22mm operators - GIC Product

Environment:
US Product

Cause:
Product Specification

Resolution:
There is no wiring diagram provided on an instruction sheet  as these units are labeled on the potentiometer itself as to which terminal is which.
Was this helpful?
What can we do to improve the information ?