Technical FAQs

Ask a Question

ATV312 drive: Why is the preset speeds not overriding the analog signal when the hand off auto control is in auto mode?

Issue:
Why is the preset speeds not overriding the analog signal when the hand off auto control is in auto mode?

Product Line:
ATV312

Environment:
All 

Cause:
Fr2 does not support the preset speed override only Fr1

Resolution:
Using Fr1 and Fr2 for auto manual the preset speeds will only override the analog signal coming in on Fr1 not Fr2 this is normal behavior. 
Was this helpful?
What can we do to improve the information ?