Technical FAQs

Ask a Question

Is arc fault CAFI available on H, J, L, M, P, R frame circuit breakers?

Issue:
Do Powerpact breakers have AFCI?
Do Powerpact breakers have arc-fault like the QO and HOM breakers?
Can H, J, L, M, P or R breakers be ordered with CAFI suffix?

Product Line:
Circuit Breakers

Environment:
Powerpact H, J, L, M, P, R Frame Circuit Breakers

Resolution:
No. Powerpact H, J, L, M, P and R breakers do not have the CAFI arc-fault function like the QO and HOM breakers. 
Was this helpful?
What can we do to improve the information ?