Technical FAQs

Ask a Question

Converting 9001KR9/SKR9 to illuminated

Issue:
Can a 9001SKR9 or 9001KR9 be converted to an illuminated operator?

Product Line:
30mm Pushbuttons - GIC Product

Environment:
US Product

Cause:
Product Charateristics

Resolution:
Yes, these operators can be converted to illuminated operators by adding a light module, and removing the liner (6512240601) from the operator.
Was this helpful?
What can we do to improve the information ?