Technical FAQs

Ask a Question

Replacement connectors for the M241 PLC.

Issue:
What are the part numbers for the replacement connectors of the M241 PLC?

Product Line:
PLC

Environment:
TM241, SoMachine

Cause:

Resolution:
The TMAT4CSET contains all the connectors required for the IO of any TM241 model.
The TMAT2PSET is the number to use to get a replacement power connector.
Was this helpful?
What can we do to improve the information ?