Technical FAQs

Ask a Question

What are the repair parts for a CH366DS Series E5(or E05) Heavy Duty Safety Switch?

Issue:
Design repair parts

Product Line:
Canadian Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:

The parts listed here are the only field replaceable parts.


Line base assembly - 4055218550 (3-required and arc suppressor assembly is included)
Load base assembly - 4055218750 (3-required)
Arc suppressor assembly - 4051270850 (3-required)
Lug assembly - 4405044601 (2 required PER base assembly)
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 4055219101 (1 required)
Line & load base mounting screws - 4020600901 (2 required PER base assembly)
Handle assembly - 4051219151
Handle Gasket - 4051126101
Handle mounting screws and washers - 2140122242(screw 2-required) and 2370100220(washer 2-required)

Door thumb retainer - 4405043301( 2 required per switch)
Door thumb screw - S1A99898 (2 required per switch)
Handle knob kit - 4028343550 (the black & red knob at the end of the handle)
Dust Shield - 4055215701 (this piece Flat, Red in color and approximately 1.16" wide by 16.10" long)
Cross bar insulator - 4055217701 (this piece is Red in color, circular in shape and approximately 4.19" long by 2.5" wide by  2.0" tall)
Cross bar insulator - 4052217801 (this piece is Red in color, circular in shape and approximately 8.85" long by 1.46" wide by 1.5" tall) 
Was this helpful?
What can we do to improve the information ?