Technical FAQs

Ask a Question

How do I configure my DI5 or DI6 input on a process drive for pulse input, and adjust the scaling?

Issue:
How do I configure my DI5 or DI6 input on a process drive for pulse input, and adjust the scaling?

Product Line:
ATV600 / ATV900

Environment:
All models, All serial numbers

Cause:
Information difficult to find in current literature.

Resolution:
We first have to configure either DI5 or DI6 as a pulse input:
From main menu, navigate to COMPLETE SETTINGS and press OK.
Navigate to SENSORS ASSIGNMENT and press OK.
Navigate to Inst. Flow Assign and press OK  
Select either DI5 or DI6 and press OK.

Once this is done, another menu option will be available:
DIx Pulse Sensor Conf.
Highlight this menu and press OK.
Your Pulse Input Low and High frequency parameters are here, as well as the Min Process and Max Process parameters.   Use these 4 parameters to adjust the scaling of your pulse train input.
 
Was this helpful?
What can we do to improve the information ?