Technical FAQs

Ask a Question

What is the coil consumption oft he CAD relays?

Issue:
Customers are checking on the consumption of the standard and low-consumption coils for CAD relays.

Product Line:
CAD TeSys And IEC Relays

Environment:
CAD Relays

Resolution:
Average Consumption at 68 °F (20 °C) and at Uc:
Vac Coil 50/60 Hz: Inrush is 70 VA / Hold-in is 8 VA
Vdc Coil: Inrush or hold-in is 5.4 Watts
CAD (Vdc) Low Consumption:  Inrush or hold-in is 2.4 Watts
Was this helpful?
What can we do to improve the information ?