Technical FAQs

Ask a Question

Can you transfer files from one ATV212 drive to another using the keypad?

 Issue:
Customer has multiple ATV212 drives and wants to copy the program from one unit to the next. 

Product line:
ATV212, Altivar 212, S-Flex

Environment:
all

Cause:
n/a

Resolution:
The VW3A1101, HMI style keypad cannot save the ATV212 program files.  To save/transfer the files the customer will need to use the Multiloader tool (part # VW3A8121) or connect to the drive using SoMove. 

 
Was this helpful?
What can we do to improve the information ?