Technical FAQs

Ask a Question

Can the ATV212 power terminals have more than one wire?

Issue
Customer wants to use more than one conductor coming into the ATV212 power terminals. 

Product Line
Altivar 212, ATV212

Environment
n/a

Cause
Parallel wiring, 2 wires per phase

Resolution
 
The wire range published for the Altivar 212 drives is for a single conductor only.  If multiple conductors are needed, use an external Power distribution block to change the multiple wires to a single conductor before coming into the drive.
Was this helpful?
What can we do to improve the information ?