Technical FAQs

Ask a Question

What is the replacement for ASISAFEMON2B?

 Issue:
Customer wants to order ASISAFEMON2B but it shows obsolete.  Do we offer a cross or replacement?

Product line:
ASISAFEMON2B Machine Safety controller AS-i

Environment:
n/a

Cause:
Obsolete

Resolution:
This model was discontinued with no replacements from Schneider Electric. 

This product was built in partnership with Leuze.  They offer the same product but contact them directly for a cross reference.
www.leuze.com
 
Was this helpful?
What can we do to improve the information ?