What is the technical details on the diagnostic relay for the ABL8RPM power supplies?
Issue:
Customer needs to know the specfication for the diagnostic relay on ABL8RPM24200
Product line:
ABL Power supplies, Quantam series
Environment:
n/a
Cause:
Literature does not show
Resolution:
The factory does not have specifications for this diagnostic relay.
The information we do have available is: Relay closed: UOut > 21.6 V
Relay contact ratings: U 230 Vac, 0.5 A max; 24 V dc, 5 mA min
Sign up for all the latest solutions, offers and best practices straight to your inbox.
All done!
Thank you for subscribing to updates from Schneider Electric.
We are excited that you have joined the group. You will receive your welcome email soon describing the program and what to expect in the upcoming weeks. Enjoy!