Technical FAQs

Ask a Question

Can we install Powerpact H breakers in a MC34206 meter stack?

Issue:
Can we mount a Powerpact H frame in a 7 jaw MC34206 stack?

Product line:
Meter Center

Environment:
600V MC stack

Resolution:
Only option is to consider using the J  frame breaker with the electronic trip (J*L36250U31X) …this can be dialed down to 100 Amps.  The H frame breaker cannot be used in the 200A meter-stacks.
Was this helpful?
What can we do to improve the information ?