Technical FAQs

Ask a Question

Are replacement coils available for the RUMC relays?

 Issue:
Customer ordered 24VAC coils and wants to replace with 24VDC

Product line:
Zelio Control RUM

Environment:
n/a

Cause:


Resolution:
The RUM relays do not have replacement parts.  Customer will need to order a new relay with the correct coil voltage.  If they have a large number to convert, they can also consider using a Control Power Transformer to change the voltages from AC to AC, or a Power Supply to change the voltage from AC to DC.
 
Was this helpful?
What can we do to improve the information ?