Technical FAQs

Ask a Question

Will the QO312ML1RB accept bolt-on QOB breakers?

Issue:
Can the the QO 3 phase load center such as QO312ML1RB, QO320ML1RB, QO330ML2RB and QO342ML2RB accept QOB bolt-on breakers?

Product Line:
Load Centers

Environment:
QO

Resolution:
No, these panels will only accept the QO plug-in breakers.
Was this helpful?
What can we do to improve the information ?