Technical FAQs

Ask a Question

Is both the transmitter and receiver included with these light curtains part numbers XUSL2E30H046N and XUSL4E30H091N?

Issue:
Are the transmitters and receivers both included with the light curtains  XUSL2E30H046N and XUSL4E30H091N?

Product line:
Light curtains

Environment:
XUSL

Resolution:
Yes, both the transmitter and receiver are included with these 2 light curtains.
Was this helpful?
What can we do to improve the information ?