Technical FAQs

Ask a Question

What is the difference between QO3RV75C and QO3RV75CG and QO3RV75CGFI?

Issue:
What is the difference between QO3RV75C and QO3RV75CG and QO3RV75CGFI?

Product line:
Power Outlet panels

Cause:
Claryfing product features differences

Resolution:
QO3RV75C comes with 1 x QO115 + 2 x QO130 + 1 x 15A + 2 x 30A 120V receptacles.
QO3RV75CG comes with 1 x QO115GFI + 2 x QO130 + 1 x 15A + 2 x 30A 120V receptacles.
QO3RV75CGFI comes with 1 x QO115GFI + 2 x QO130GFI + 1 x 15A + 2 x 30A 120V receptacles.

 


 
Was this helpful?
What can we do to improve the information ?