Technical FAQs

Ask a Question

Root element is missing error then the Scadapack work bench will crash

Problem description:  There were 3 customer programs that are having an issue with the Scadapack workbench program when you right click on the Resource1 program>select IO Device. An error will occur about Root element is missing.

Corrective action: The file Instance_of_Device.xml is corrupted on the programs. For example the program BORE1P_02. This file should be under the resource folder SCADAPack300E\BORE1P_02. Delete this file, then open the project in Scadapack Workbench, and then try opening I/O device window. The problem should be corrected.
Or see attached file.

 
Was this helpful?
What can we do to improve the information ?