Technical FAQs

Ask a Question

Can the QOU breaker be used with 480V application?

Issue:
480V application for QOU breaker

Product Line:
Breaker

Environment:
QOU Breaker

Resolution: 
No, the QOU breaker cannot be used with 480V application. An H frame breaker can be used for this application, however it is larger and would need a mounting kit (S29305) to be mounted on DIN rail.
Was this helpful?
What can we do to improve the information ?