Technical FAQs

Ask a Question

Why does my Process Drive only show Ignore under 4-20ma loss?

Issue:
Why does my Process Drive only show Ignore under 4-20ma loss?

Product Line:
Altivar Process Drive

Environment:
ALL

Cause:
Wiring / Programming

Resolution:
Under Complete Settings > Input/Output > in the AI/AQ Tab, ensure that AI2 or AI3 is set to Type=Current, Min Value = 4ma
Now go to Complete Settings > Error/Warning Handling > 4-20ma Loss and under AIx you should now see other options like per Stop Type and Fallback speed
 
Was this helpful?
What can we do to improve the information ?