Technical FAQs

Ask a Question

PM5560 wiring diagram change for 2VT 3PH3W connection

Issue
PM5560 wiring diagram change for 2VT 3PH3W connection

Product Line
PM5560 series meter

Environment
Installation Guide

Cause
There is a mistake in the wiring diagram for the PM5560 2VT 3PH3W connection.

Resolution
Please refer to the attached modified draft diagram, which will be corrected in an upcoming installation guide. Suggest the customer to modify the wiring connection as per the attached diagram.
Was this helpful?
What can we do to improve the information ?