Technical FAQs

Ask a Question

Towerlight scangroup in Vijeo Designer is pointing to the wrong equipment

Issue:
Towerlight scangroup in Vijeo Designer is pointing to the wrong equipment

Product Line:
Vijeo Designer V6.1 SP1 or greater

Resolution:
If the Towerlight scangroup in Vijeo Designer is ever pointing to another equipment in your application, it is likely that the internal IDs have been mixed up. In order to resolve this, delete the Towerlight driver, add it back, delete it, and add it back. Usually this will clear up the mixed up internal IDs. You may need to try a few times if you have many equipment configured in your application.
 
Was this helpful?
What can we do to improve the information ?